ATI Industrial Automation   ATICombinedDAQFT .NET Class Library  

Visit our website.

SetTorqueUnits( torqueUnits As String ) As Integer

Sets the units of the torque outputs.

Arguments

torqueUnits

In: The units to output torques in. Acceptable values are "in-lb","ft-lb","N-m","N-mm","kg-cm".

Returns

0: successful completion
1: Calibration not initialized (call LoadCalibrationFile before calling this function)
2: invalid units specified<

See Also

LoadCalibrationFile